Our website uses cookies to provide you with the best possible service. More information about the use of cookies on this website and how they can be disabled is available on our information page. With your consent, you confirm that you have read the information about the use of cookies and accept it. Please also note our further information on the subject of data privacy policy.

TDK TDK Electronics · TDK Europe

Ferrite Magnetic Design Tool

The MDT software allows application-related parameters to be calculated for all available EPCOS ferrite cores and / or materials. It provides access to their digitized material data including their graphical representations. The user manual of the software contains a detailed description of all functions. The tool can be used as online version, tested in browsers like Google Chrome, Mozilla Firefox, Internet Explorer and Opera, or as download, developed for Windows 7 and 10. The online version does not offer the same comprehensive set of functions as the desktop version.

The ferrite material list was updated according to the EPCOS Data Book 2017 “Ferrites and Accessories”. The new high frequency material PC200 was added.

Among the features of the current MDT version are:

  • Simulations based on user-defined core parameters
  • Database expanded to include Steinmetz coefficients for power losses
  • Display of complex permeability and impedance as a function of frequency
  • Transmittable power adjusted for skin and proximity effects (from the wire calculation menu)
  • Calculation of the distortion factor (third harmonic) under specific circuit conditions at various temperatures
  • Calculation of core loss as a function of signal form
  • Specification of wire thickness as per American Wire Gauge (AWG)

To support design-ins you will find the data sheets for all materials by applications under www.tdk-electronics.tdk.com/ferrite_materials.

Launch the online version keyboard_arrow_right

Download Program [7.0 MB]keyboard_arrow_right